AutomationDirect Customer Forum  

Welcome to the AutomationDirect Customer Forums.
These forums are intended as a place for AutomationDirect customers to help one another, share information, and share ideas.
The forums are not routinely monitored by AutomationDirect Technical Support staff. While staff members may answer questions occasionally, for a prompt response to a problem please contact Technical Support directly at: 1(800) 633-0405 or (770) 844-4200 or e-mail Tech Support.


Go Back   AutomationDirect Customer Forum > General Applications

Reply
 
Thread Tools Rate Thread Display Modes
  #1  
Old 11-03-2009, 11:53 AM
MAGOO5150 MAGOO5150 is offline
Registered User
 
Join Date: Nov 2009
Posts: 3
C-More to 5/04

I am fairly new to the C-more line of products and have a question. I am trying to connect an EA7-T8c panel to a AB 5/04. Everything works fine connected with the 3 meter cable (EA-SLC-232-CBL), but I need to located this panel about 30 feet away from the PLC, the 5/04 does not have the RJ45 jack theat the previous models did. Any suggestions
Reply With Quote
  #2  
Old 11-03-2009, 03:01 PM
KPrice KPrice is offline
Registered User
 
Join Date: Apr 2001
Location: Oley, PA
Posts: 645
MAGOO5150, as far as a supplier for D-sub connectors, I suggest trying
http://www.l-com.com
You can save yourself soldering (or crimping) D-sub connectors by using the AutomationDirect Ziplink modules and using standard cables with molded-on D-sub connectors. RS232 can go about 50ft. Use good shielded cable. Is this what you're looking for?
Reply With Quote
  #3  
Old 11-03-2009, 03:14 PM
jackson jackson is offline
Registered User
 
Join Date: May 2003
Posts: 333
If the run ends up being longer than the specified 50 feet, you could always put an FA-ISOCON at the PLC side and use RS-422.
The C-more panel doesn't need the ISOCON because it has RS-422/485 built in (unless you just want total isolation on the network run).
Reply With Quote
  #4  
Old 11-04-2009, 11:02 AM
MAGOO5150 MAGOO5150 is offline
Registered User
 
Join Date: Nov 2009
Posts: 3
Thanks, for the quick replies. I figured I would have to make up a cable but wasnt sure about the length. Again thanks
Reply With Quote
Reply

Thread Tools
Display Modes Rate This Thread
Rate This Thread:

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is On

Forum Jump


All times are GMT -4. The time now is 06:08 PM.


Powered by vBulletin® Version 3.8.4
Copyright ©2000 - 2009, Jelsoft Enterprises Ltd.