AutomationDirect Customer Forum  

Welcome to the AutomationDirect Customer Forums.
These forums are intended as a place for AutomationDirect customers to help one another, share information, and share ideas.
The forums are not routinely monitored by AutomationDirect Technical Support staff. While staff members may answer questions occasionally, for a prompt response to a problem please contact Technical Support directly at: 1(800) 633-0405 or (770) 844-4200 or e-mail Tech Support.


Go Back   AutomationDirect Customer Forum > General Applications

Reply
 
Bookmark and Share Thread Tools Rate Thread Display Modes
  #1  
Old 04-29-2012, 08:29 AM
alvmatos alvmatos is offline
Registered User
 
Join Date: Jul 2010
Posts: 1
Unhappy Ti 305-04b / ad- d3-10b-1

I have a Texas Instruments Base Series 305-04B/05B working with a DL 350 CPU, and I replace the TI base for a new Automation Direct D3-10B-1. PLC steel runs but some of the Output cards not works. Is this a base issue or the configuration or some thing also?
Reply With Quote
  #2  
Old 04-30-2012, 10:50 AM
scott.lawrence scott.lawrence is offline
Registered User
 
Join Date: Feb 2011
Location: New Castle,Pa
Posts: 300
If the D3 series is like the 205s, then you have to configure the cards in the program.
Reply With Quote
  #3  
Old 05-01-2012, 09:46 AM
KB1GNI KB1GNI is offline
Registered User
 
Join Date: Mar 2011
Location: Live Free or Die, USA
Posts: 62
The 305-04B is a 10 slot rack and the 305-05B is an 8 slot rack. Which did you have?

305 addressing is slot-dependent, not software-dependent. However, there is a jumper on the backplane of the 10-slot racks that changes the addressing of slot 10.

It would help to have a list of part numbers and physical layout of the cards in the rack, as well as what your program is set up for as far as addressing.

The manual is invaluable as far as determining addressing, especially if you are not familiar with the GE Series One/TI/Siemens/DL305 series. Sometimes, even if you are!
__________________
-Lee

“Felix, qui potuit rerum cognoscere causas” - Happiness is understanding how things work.
Reply With Quote
Reply

Thread Tools
Display Modes Rate This Thread
Rate This Thread:

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is On

Forum Jump


All times are GMT -4. The time now is 09:12 PM.


Powered by vBulletin® Version 3.8.6
Copyright ©2000 - 2013, Jelsoft Enterprises Ltd.