AutomationDirect Customer Forum  

Welcome to the AutomationDirect Customer Forums.
These forums are intended as a place for AutomationDirect customers to help one another, share information, and share ideas.
The forums are not routinely monitored by AutomationDirect Technical Support staff. While staff members may answer questions occasionally, for a prompt response to a problem please contact Technical Support directly at: 1(800) 633-0405 or (770) 844-4200 or e-mail Tech Support.


Go Back   AutomationDirect Customer Forum > AC Drives, Stepper, and Servo Applications

Reply
 
Thread Tools Rate Thread Display Modes
  #16  
Old 10-31-2009, 06:43 PM
milldrone milldrone is offline
Registered User
 
Join Date: Jan 2005
Location: Anderson Ca.
Posts: 552
Quote:
Originally Posted by bfitz View Post
My thoughts are that you could probably do the first level tune (P0.05 set to 01) with the load connected. I believe that this test doesn't actually move the motor (_please_ wait for confirmation on this though).
Unfortunately I'm not at work so I cannot confirm if the #1 auto tune does not move the motor.

I know for a fact that the ABB ACS800 has two different autotunes. One with no load connected to the motor, this one is needed for ultra low speed (1 & 2 hz) response. The other does not move the motor, and can be used for most other non critical control. But this does nothing to help you.

ABB reps have told me that their sensorless vector is the best (can you imagine that!) and that some "sensorless vector drives" are not much more than torque boost. I cannot confirm either way. I suspect there is some truth here.

I believe that Brian is right (except for one little caveat)

Quote:
Originally Posted by bfitz View Post
This is critical. You are changing the load on the drive. A V/Hz drive will just keep putting out voltage at the specified frequency without knowing that the motor slip is decreasing rapidly. An S-curve will help you approach a set speed with minimal drama, but the situation you referenced is encountered at a steady state. S-curves won't help you here.
I believe that some drives (low end sensorless vector) actually increases the frequency in an attempt to keep the motor speed the same as the desired speed. When the load is gone suddenly and the speed is "high" there is a potential for overvoltage. Because the drive will then try to reduce the frequency to keep the motor speed equal to the desired speed.

You mentioned earlier that this was a high inertia load. Did you make any adjustments in the P 2.00 to P 2.05 area?
__________________
Vaughn

Last edited by milldrone; 10-31-2009 at 06:52 PM.
Reply With Quote
  #17  
Old 10-31-2009, 07:15 PM
bfitz bfitz is offline
Registered User
 
Join Date: Dec 2008
Location: Nebraska
Posts: 155
Quote:
Originally Posted by milldrone View Post
I believe that some drives (low end sensorless vector) actually increases the frequency in an attempt to keep the motor speed the same as the desired speed. When the load is gone suddenly and the speed is "high" there is a potential for overvoltage. Because the drive will then try to reduce the frequency to keep the motor speed equal to the desired speed.
I'm not an expert on VFDs, but I believe what you are talking about is called slip compensation. The frequency output can vary to keep the motor speed equal to the desired speed regardless of load on the motor, or slip. Yes, when the load is gone suddenly, the motor has more torque than necessary and slip starts to decrease and the extra energy is put into speeding up the connected load. However, I would wager that a sensorless vector VFD would be able to detect this increase in speed and compensate by lowering the output frequency almost instantly. This should prevent an overvoltage by limiting the amount of extra energy stored in the rotating mass in the form of overspeed. In my mind, this is exactly the purpose of slip compensation; well, that and minimizing speed errors in general.

Brian
Reply With Quote
  #18  
Old 11-02-2009, 11:14 AM
milldrone milldrone is offline
Registered User
 
Join Date: Jan 2005
Location: Anderson Ca.
Posts: 552
Quote:
Originally Posted by bfitz View Post
I'm not an expert on VFDs, but I believe what you are talking about is called slip compensation. The frequency output can vary to keep the motor speed equal to the desired speed regardless of load on the motor, or slip. Yes, when the load is gone suddenly, the motor has more torque than necessary and slip starts to decrease and the extra energy is put into speeding up the connected load. However, I would wager that a sensorless vector VFD would be able to detect this increase in speed and compensate by lowering the output frequency almost instantly.
Yes you are correct. This is merely slip compensation. This is also ABB's point (it's merely slip compensation) and the "almost instantly" part also.

Check out what the drive does to the defaults on P 2.01 (slip compensation page 4-25) when in vector mode.

Edit: I'm hoping to have some time this afternoon to try the #1 auto tune on one of my units.
__________________
Vaughn
Reply With Quote
  #19  
Old 11-02-2009, 03:57 PM
milldrone milldrone is offline
Registered User
 
Join Date: Jan 2005
Location: Anderson Ca.
Posts: 552
bblank,

I just tried a #1 auto tune on a early firmware version GS3. It does not move the motor and takes about 1/2 second to perform the test.

To perform a #1 auto tune on my only current firmware GS3 I would have to put on my fall protection gear, and separate an integral motor from it's gearbox. I'm not wanting to do that!
__________________
Vaughn
Reply With Quote
Reply

Thread Tools
Display Modes Rate This Thread
Rate This Thread:

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is On

Forum Jump


All times are GMT -4. The time now is 05:59 PM.


Powered by vBulletin® Version 3.8.4
Copyright ©2000 - 2009, Jelsoft Enterprises Ltd.