AutomationDirect Customer Forum  

Welcome to the AutomationDirect Customer Forums.
These forums are intended as a place for AutomationDirect customers to help one another, share information, and share ideas.
The forums are not routinely monitored by AutomationDirect Technical Support staff. While staff members may answer questions occasionally, for a prompt response to a problem please contact Technical Support directly at: 1(800) 633-0405 or (770) 844-4200 or e-mail Tech Support.


Go Back   AutomationDirect Customer Forum > Communications

Reply
 
Thread Tools Rate Thread Display Modes
  #1  
Old 11-03-2009, 12:29 PM
emabond emabond is offline
Registered User
 
Join Date: Sep 2007
Posts: 9
RS-485 "network"

I need to set up an RS-485 network with 2 devices and a DL260. Physically, they are all located in the same cabinet. The 2 devices have a DB9 connector, and the DL260 has the high density 15 pin connector.

What is the best way to network them together? Will 3 pigtails work? Skip the 120 ohm resistors since there is no 120 ohm cable? Should I use a CMA15 and try to find somebody who makes a CMA9?

Any thoughts on the best way to do this are greatly appreciated.

Thanks!
Reply With Quote
  #2  
Old 11-03-2009, 12:52 PM
bcarlton bcarlton is offline
Registered User
 
Join Date: Dec 1999
Location: Yakima, WA
Posts: 1,597
http://www.automationdirect.com/adc/...t)/ZL-RTB-DB09
__________________
thePLCguy
Reply With Quote
  #3  
Old 11-03-2009, 05:24 PM
KPrice KPrice is offline
Registered User
 
Join Date: Apr 2001
Location: Oley, PA
Posts: 645
emabond, a compact installation, but tedious to make, would be to use (2) pigtails and a solder (or crimp) D-sub connector. Use a 15-pin HD pigtail for the PLC, and go the the 1st device and solder the 15-pin HD and a 9-pin pigtail to a solder (or crimp) D-sub connector. This would create your daisy-chain configuration. Yes, you can skip the end-resistors because your length is short. (3 pigtails would not give you a daisy-chain configuration.)

If you find a "CMA9", let me know. I have not be able to find this. L-com carries a 9pin/terminal-block adapter, but it is bulky and too big to hang on a port.
Reply With Quote
Reply

Thread Tools
Display Modes Rate This Thread
Rate This Thread:

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is On

Forum Jump


All times are GMT -4. The time now is 06:09 PM.


Powered by vBulletin® Version 3.8.4
Copyright ©2000 - 2009, Jelsoft Enterprises Ltd.