AutomationDirect Customer Forum  

Welcome to the AutomationDirect Customer Forums.
These forums are intended as a place for AutomationDirect customers to help one another, share information, and share ideas.
The forums are not routinely monitored by AutomationDirect Technical Support staff. While staff members may answer questions occasionally, for a prompt response to a problem please contact Technical Support directly at: 1(800) 633-0405 or (770) 844-4200 or e-mail Tech Support.


Go Back   AutomationDirect Customer Forum > Operator Interface

Reply
 
Thread Tools Rate Thread Display Modes
  #1  
Old 10-28-2009, 12:30 PM
Fuzzy Fuzzy is offline
Registered User
 
Join Date: Oct 2009
Posts: 1
Cmore and dll error

I have just started having problems with the C-more programming software. the error I get is "EA-PGM.exe has encountered a problem and needs to shut down". The "Error signature" has the following information AppName:ea-pgm.exe, AppVer:2.53.0.0, ModName: mfc42u.dll, ModVer: 6.2.4131.0, Offset: 00004847. I was having this problem with ver2.4 so I upgraded to ver2.53. I have tried downloading mfc42u.dll with no luck. Any help would be very appreciated.
Reply With Quote
  #2  
Old 10-29-2009, 10:12 AM
HMI Eng HMI Eng is offline
Registered User
 
Join Date: May 2006
Posts: 376
Did the C-more software ever work on that particular PC? If so, then it is likely that about the time it stopped working, something was installed or uninstalled on the PC that corrupted the mfc42u.dll . We have had issues trying to reinstall this DLL also.

Unfortunately the only solution we have found is reinstalling the Service Packs. If this does not work, then reinstalling the OS on the PC.

There may be some way to get the correct mfc42u.dll in the right place, but we have not been able to.
Reply With Quote
  #3  
Old 10-29-2009, 01:25 PM
a agnone a agnone is offline
Registered User
 
Join Date: May 2004
Location: Williamsport, PA 17701
Posts: 609
Smile

Has anyone tried going to a working computer and search for the file. I am running XP and had to go to another computer and found the file in several locations. It was in windows/system 32, and some other places. I took it from one computer and copied it onto the other computer. I may have copied it into several directories to make sure it would work. But it may only need to be in the system32 directory. I can not remember where I copied it to, it was long ago.
Reply With Quote
  #4  
Old 10-29-2009, 03:18 PM
Tubecut Tubecut is offline
Registered User
 
Join Date: Jun 2003
Location: Georgiana, AL.
Posts: 239
Quote:
Originally Posted by HMI Eng View Post
reinstalling the OS on the PC.
Such a drastic fix! That seems to be the standard response from any software vendor when the products fail.

It is like a doctor telling you that you have cancer, it can be cured, just reinstall your self, get born again and you are cured.

It would seem that the software providers should/could be able to allow there package to be repaired?
Reply With Quote
  #5  
Old 10-30-2009, 10:15 AM
HMI Eng HMI Eng is offline
Registered User
 
Join Date: May 2006
Posts: 376
I agree; it is drastic. In this case, it is not the C-more package that is broke. The DLL is a Windows file used by C-more. It is not installed with C-more. fficeffice" />>>
Reply With Quote
  #6  
Old 10-30-2009, 05:01 PM
Tubecut Tubecut is offline
Registered User
 
Join Date: Jun 2003
Location: Georgiana, AL.
Posts: 239
DLL error(s)

These DLL errors are always getting messed up, but I am thinking here it seems to only effect the application program itself.

I have had a similar problem on a desktop that I can't upgrade the Cmore software. So, I use my laptop for that work and the desk top for other things.
Makes me leery of upgrading to Windows 7

If the DLL only effects the application program, isn't there some way to have a way around that?
Reply With Quote
Reply

Thread Tools
Display Modes Rate This Thread
Rate This Thread:

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is On

Forum Jump


All times are GMT -4. The time now is 05:53 PM.


Powered by vBulletin® Version 3.8.4
Copyright ©2000 - 2009, Jelsoft Enterprises Ltd.