AutomationDirect Customer Forum  

Welcome to the AutomationDirect Customer Forums.
These forums are intended as a place for AutomationDirect customers to help one another, share information, and share ideas.
The forums are not routinely monitored by AutomationDirect Technical Support staff. While staff members may answer questions occasionally, for a prompt response to a problem please contact Technical Support directly at: 1(800) 633-0405 or (770) 844-4200 or e-mail Tech Support.

For product questions, start here: Online Manuals and Product Inserts


Go Back   AutomationDirect Customer Forum > General Applications

Reply
 
Bookmark and Share Thread Tools Rating: Thread Rating: 2 votes, 5.00 average. Display Modes
  #1  
Old 12-20-2007, 03:37 PM
BigJames240 BigJames240 is offline
Registered User
 
Join Date: Dec 2007
Location: Enterprise, AL 36330
Posts: 1
12v delay-off timer

I am in need of an inexpensive 12v off-delay timer. Nothing too elaborate; simply 12v, off-delay, and small. Any suggestions would be greatly appreciated. I am not 'timer savvy' so please be as detailed as possible with any replies.

Thanks!
James
Reply With Quote
  #2  
Old 12-21-2007, 10:42 AM
elevmike elevmike is offline
Registered User
 
Join Date: Aug 2003
Location: Detroit, MI, USA
Posts: 454
James,

You might not find a 12vdc off delay timer.. However, A small 12vdc relay, a diode, a capacitor & a resistor would do the trick. All available at your local Radio Shack.

without the relay contact load & delay time, I cant help you with the exact parts.

Reply With Quote
  #3  
Old 12-21-2007, 12:32 PM
milldrone milldrone is offline
Registered User
 
Join Date: Jan 2005
Location: Willows Ca.
Posts: 1,121
BigJames240,

This doesn't fit your inexpensive criteria, but here are some omron units. I think you can buy a DL05 DC unit (D0-05DD-D) for less money.

signal off delay programmable
H5CX-ASD
H5CX-L8D
H5CX-AD
H3CR-A

Here is a koyo unit that will work on 12 volts
KT-V4S-C-D
It's also a signal off delay

A word of warning: if this is going on an 12 volt system that is also starting an engine you will need some protection if you decide to use a plc.

I couldn't find any 12 volt true power off delay units

Vaughn

[This message has been edited by milldrone (edited 12-21-2007).]
__________________
PERCUSSIVE MAINTENANCE: The fine art of whacking the devil out of an electronic device to get it to work again.

Vaughn
Reply With Quote
Reply

Thread Tools
Display Modes Rate This Thread
Rate This Thread:
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
All times are GMT -4. The time now is 03:41 PM.


Powered by vBulletin® Version 3.8.6
Copyright ©2000 - 2015, Jelsoft Enterprises Ltd.