AutomationDirect Customer Forum  

Welcome to the AutomationDirect Customer Forums.
These forums are intended as a place for AutomationDirect customers to help one another, share information, and share ideas.
The forums are not routinely monitored by AutomationDirect Technical Support staff. While staff members may answer questions occasionally, for a prompt response to a problem please contact Technical Support directly at: 1(800) 633-0405 or (770) 844-4200 or e-mail Tech Support.

For product questions, start here: Online Manuals and Product Inserts


Go Back   AutomationDirect Customer Forum > General Applications

Reply
 
Bookmark and Share Thread Tools Rate Thread Display Modes
  #1  
Old 05-21-2012, 01:38 PM
Samuraimarc Samuraimarc is offline
Registered User
 
Join Date: May 2012
Posts: 1
Arrow Running Directsoft 5 Under WINE

Hello all,
I'm going to post yet another Linux question to run DS5 under WINE.
Here's what I'm running:

Lenovo ThinkPad T61 Laptop
Linux Distro: Debian Squeeze 6.05
Wine v1.01
Direct Logic 05 #D0-05DR
Serial Communication

I am aware of the compatibility list for DirectSoft 5 and AD software. I am capable of running the software in virtual box but that just brings me back to the frustration of window’s.

I can successfully run the software in wine if I adjust the DS500.ini COM*ENABLE= to 0’s. I have tried linking the ttyS0 to com2 (symbolically) with the COM2ENABLE=1 in the .ini and the program hangs.
Link code:

Code:
 ln -s /dev/ttyS0 /~/.wine/dosdevices/com2
I have also changed the permissions of ttyS0 to 0644 with:

Code:
 chmod 0644 /dev/ttyS0
And the program starts, and runs but will not communicate with the PLC. I am running OP-WINEDIT Optimate configuration software just fine in wine with com2 linked to ttyS0.

There was a post back in 2006 about this and they did it using Ethernet. As that’s not an option for the D0-05DR I need to get the serial working.
Can anybody throw me a bone who is Linux savy?
Thanks in Advance.
Reply With Quote
Reply

Thread Tools
Display Modes Rate This Thread
Rate This Thread:
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
All times are GMT -4. The time now is 10:40 AM.


Powered by vBulletin® Version 3.8.6
Copyright ©2000 - 2015, Jelsoft Enterprises Ltd.