Announcement

Collapse
No announcement yet.

Programming GS1 Drive to automatically go to desired settings after pressing run

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Programming GS1 Drive to automatically go to desired settings after pressing run

    How do I program my GS1 Drive to go to a desired frequency after pressing run? I don't want to have to set the frequency/RPM manually using the potentiometer nor up/down keys after pressing run. I am using the GS1 drive to control a motor for a positive-displacement pump. Should I disable Line Start Lockout (P6.30)? Or do I need to use an analog input and change the source of operation for the frequency command in order to do this?


  • #2
    you could wire one of the DIs then setup that DI to be apreset speed. (Atleast maybe, if the GS1 allows the preset speed inputs)

    Comment

    Working...
    X