Announcement

Collapse
No announcement yet.

Communication between Emerson EP206-P and C-more EA9 HMI

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Communication between Emerson EP206-P and C-more EA9 HMI

    I have connected an Emerson Drive EP206-P with C-more EA9 via Modbus TCP/IP. I can see the boolean bits on the HMI, but the value of the Jog speed is not shown correctly. The Data type that I'm trying to use to see the value is BCD int32. The jog speed value on the driver is 408 in/m but the HMI show 198 in/m. Someone that can help with this issue. Thanks in advance !!


  • #2
    You have the wrong data type selected. You should be using Signed_Int_32.
    If you have an urgent issue, please contact AutomationDirect's Technical Support team.

    AutomationDirect.com Technical Support: 1(800) 633-0405 or (770) 844-4200 Email Tech Support

    Comment



    • #3
      Thanks Do-More PE for your help! I'll check that option. I'll let you know the results.

      Comment

      Working...
      X