Announcement

Collapse
No announcement yet.

GSeDRV100 and GSoft

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts


  • GSeDRV100 and GSoft

    I can't access the GS2 drive via my ethernet connection and GSoft. Aren't I supposed to be able to do that?


  • #2
    The manual for the interface does not mention using the GSoft software. It provides Modbus TCP/IP accessibility to the PLCs listed. Also the description for GSoft describes serial connections only.
    Last edited by bcarlton; 05-30-2019, 09:18 AM.
    thePLCguy

    Bernie

    Comment



    • #3
      Originally posted by bcarlton View Post
      The manual for the interface does not mention using the GSoft software. It provides Modbus TCP/IP accessibility to the PLCs listed. Also the description for GSoft describes serial connections only.
      I thought I was missing something in the manual. Obviously, I was. Thank you.

      Comment

      Working...
      X