Announcement

Collapse
No announcement yet.

Modbus with Arduino

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Modbus with Arduino

    I am wanting to control my GS2 drive with an Arduino sending a frequency command to the drive over rs485. The Arduino will have a PID controller. I know the GS2 drive has a PID controller but I kneed more control that I can do with the VFD. I can program basic stuff with the Arduino but I need a little help with this code. I will be including the <ModbusMaster.h> library or if somebody has a better one let me know. Also would like to read the frequency from the dive as I am also planning on connecting a display to the Arduino.

    I would like to know the settings I need to set on the VFD and also some example code that I could copy and past. That is well explained and then I can possibly be able to build it from there.

    Benjamin
Working...
X