Announcement

Collapse
No announcement yet.

Gs1 error

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts


  • Gs1 error

    I have a Gs1, runs great but all the sudden i have a EF fault on the screen, and I can't reset it. Someone help.
    Thank you, Bob


  • #2
    I've never used a GS1 but it looks like an external fault. Look at parameter 3.02 which is how that terminal's function is programmed.

    Comment



    • #3
      Originally posted by sii View Post
      I've never used a GS1 but it looks like an external fault. Look at parameter 3.02 which is how that terminal's function is programmed.
      In addition to checking the programming check to see what digital inputs DI3 or DI4 are wired to, there may be some sort of machine protection wired to them.
      Futti Utu

      Comment



      • #4
        Thank you, but now how do I erase the error code.

        Comment



        • #5
          I would assume that once you remove the signal being sent as an external fault you should be able to reset the drive

          Comment

          Working...
          X