Announcement

Collapse
No announcement yet.

gs4 switch

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • gs4 switch

    need help with wiring a forward reverse switch on a gs4. could someone please provide some input
    thanks

  • #2
    Can you provide more information on the application?

    Comment


    • #3
      need to install a mechanical forward/reverse switch on analog terminals, this is for a metal lathe.
      i will eventually figure it out. just seeing if someone has already jumped thru hoops with gs4 programming
      with lack of info in manual on how to install and program switch.

      i am sure it is very simple.

      thanks



      Comment


      • #4
        currently in local mode, my pot switch is turning on the motor. i do not want to use the pot as a switching device.
        hence the installation of forward/reverse switch.

        Comment


        • #5
          Look at the FWD & REV terminals on page 2-37 and parameters 3.00 & 3.02.

          Comment


          • #6
            finally got it working after a few hours of beating my head.

            local mode switch working
            forward and reverse switch working
            pot working
            just have to connect switch for jog forward/reverse

            thanks

            Comment

            Working...
            X