Announcement

Collapse
No announcement yet.

400 Volt 3 phase Motor

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • 400 Volt 3 phase Motor

    im considering an old 400 V, 3/4 hp 3 phase motor to run my wood lathe using a VFD for speed control and reversing
    is this feasible?

  • #2
    If it is an old motor, make sure it is rated to run on a VFD and at low speeds.

    Comment


    • #3
      this motor was built way before vfd's! it even has a cast iron centre section with cast in "feet"

      Comment


      • #4
        Unless there is something special about the mounting a 3/4hp motor shouldn't be too expensive to replace, which probably would be best. But with short motor leads and/or a load reactor, and conservative operating conditions I imagine the old motor would probably work ok, I have seen a number on non-inverter rated motors working fine on an inverter

        Comment


        • #5
          there's nothing special about the motor other than its age and origin. plus trhe fact that my entire wood working shop is all antique equipement and motors and i like it like that!
          so im looking for suggestions regarding a vfd for it, i know nothing about them

          Comment


          • #6
            I would suggest using an output reactor with the VFD. The old motor should be fine then.

            Comment

            Working...
            X