Announcement

Collapse
No announcement yet.

SVA-2040 & SVL-204 Cannot select Motor Code 12

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • SVA-2040 & SVL-204 Cannot select Motor Code 12

    Hi folks, I hope you can help.
    I just purchased a SVA-2040 Drive and a SVL-204 motor to go along with it.
    When attempting to set the P1-31 Motor Code to 12, it reverts back to 10.
    Whatever I try, 12 does not stick.
    All other parameters seem to apply OK. The directions are correct, the homing is attempting as normal (just very low torque from the motor).
    I have it configured to Home @ power up, make the limit then back off to the "Z".
    I've killed the power between settings, no effect.
    If I enter 12 to P1-31, then go right back to it, it is back to 10.
    Any help greatly appreciated.
    Thanks,
    Sawyer

    edit: meant to include drive Firmware 2.105,
    Thanks
    Last edited by Sawyer; 03-02-2020, 10:52 PM.

  • #2
    OK now, all sorted.
    Auto enable was selected.
    Needed to disable the drive in order to change the setting.
    Good to go now,
    thanks

    Comment

    Working...
    X