Announcement

Collapse
No announcement yet.

H2-DM1E and ethernet

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts


  • H2-DM1E and ethernet

    Hello all,

    I cant seem to connect H2-DM1e to my router
    Click new connection
    ethernet in the link wizard
    Udp/p
    No mac adress in default adapter but shows up when switched to intel 8256lf-2
    IP shows 255.255.255.255
    Query blinks Eth led
    click next
    error connecting to PLC
    Ext error: Timeout error

    netedit shows same data when I switch from default adapter to intel
    I have tried different computers and different cables. Runing windows 7

    Anyone have an idea of what is going on?

    I have no trouble connecting via USB

    Thanks,
    TJ


  • #2
    Use NetEdit to assign the DM1E's IP Address along with its subnet mask. You can also do it from within Do-more Designer using the USB link (PLC->System Information, then in the lower middle is the Set Node and IP Configuration button to configure those settings).

    Make sure your IP Address and Subnet Mask are consistent with the PC running Designer. Once you have the PLC's IP Address and subnet mask established, then you should be able to create an Ethernet link using the Link Wizard from Designer.
    There are 10 kinds of people in this world, those who know binary, and those who do not.

    Comment



    • #3
      That was it; works now
      Thanks

      Comment

      Working...
      X