Announcement

Collapse
No announcement yet.

CLICK PLC communication with LookoutDirect

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • CLICK PLC communication with LookoutDirect

    Has anyone got the CLICK PLC to communicate with Lookout Direct?

    Im using the rs232 to usb cable from the CLICK to PC.

    I double checked all settings when defining LINK

    PORT2
    baud rate: 38400
    Address: 1
    Parity bit: odd
    Bits: 8
    Stop Bit: 1

    Tried all available protocols from Lookout
    Any help would be appreciated.

    Troy


  • #2
    Are these the same setting that the Click software is using? The only appropriate protocol (unless thee is one specifically labeled 'Click') would be Modbus.
    thePLCguy

    Bernie

    Comment



    • #3
      I have had no issue working with Lookout on the Modbus driver from the RS232 ports or RS485 port.

      Verify your settings and connection.
      Water and Wastewater Telemetry
      Consult.Develop.Solve.

      Comment

      Working...
      X