Announcement

Collapse
No announcement yet.

DoMore and MB-Gateway

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • DoMore and MB-Gateway

    Hello, I'm using MB-Gateway connected to DoMore CPU to communicate with ABB Drive. For testing I have set up two drives, connected on RS-485 to the MB-Gateway and I'm using MRX and MWX functions in DoMore to read and write to and from the drives. All works well until one of the drive drops from the bus (powerfailure or something that would cause the drive to stop communicating). Then I get an error on the MB-Gateway and also lose communication to the other drive. What is there to be done ?

    Best regards

    Guğmundur

  • #2
    For anyone interested, Gudmundur Ben also posted this on Host Engineering's forum where folks are answering him. See --> http://forum.hosteng.com/index.php/topic,2048.0.html
    Greg Kiser
    Hos Engineering, Inc.
    support@hosteng.com
    http://forum.hosteng.com
    This isn't all true.

    Comment


    • #3
      Thanks Greg. I would have missed the HOST forum post for some time.

      Comment

      Working...
      X