Announcement

Collapse
No announcement yet.

sitelink router questions

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • sitelink router questions

    Is the 5gb monthly limit for all traffic through the router, or just utilizing the vpn?

    Will it work with Verizon? or ATT only.

  • #2
    All data that passes from the client to the router through the Stride SiteLink cloud (see https://cdn.automationdirect.com/sta...kvpnrouter.pdf pg 7) counts towards the 5GB monthly limit except data that is used in the data logging subscription (SE-SL010, SE-SL011, SE-SL012). In addition, the 5GB limit is shared across all SiteLink routers in a specific company account. After 5GB, the data is throttled until the next month. Additional data bandwidth can be purchased if desired through your Stride SiteLink account (SE-SL030, SE-SL031, SE-SL032).

    No, the 4G model is designed to only operate on AT&T's network.

    Comment

    Working...
    X