Announcement

Collapse
No announcement yet.

Programming Port

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Programming Port

    Is there any way to change the programming port (9999) for programming with the Productivity Series PLCs and the C-more HMIs? Looks like I can change the port for the web server, remote access, etc, but the programming port seems stuck.


  • #2
    Both are set to 9999 and are not configurable. However if you need to access through a router using port forwarding look at P058 in productivity help file and CM132 in the Cmore help file.

    Comment



    • #3
      Originally posted by PSeries_Eng View Post
      Both are set to 9999 and are not configurable. However if you need to access through a router using port forwarding look at P058 in productivity help file and CM132 in the Cmore help file.
      @OP: Just remember not to expose your programing port to the whole internet without some sort of authentication interface in between. It would be better to have a VPN with the proper encryption and login to get you into the machine's network and then access the programming interface from inside the VPN.

      Comment

      Working...
      X