Announcement

Collapse
No announcement yet.

P2-550 CPoe To a Laser Marker

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • P2-550 CPoe To a Laser Marker

    I am using a CPoE to talk to a Laser Marker. I get the .TCPConnected Bit and No errors But the Laser uses String commands and needs A CarrageReturn and Line Feed to end the string. How can I pack into the cmd string the CarrageReturn and Line Feed to send??????


  • #2
    See example code and what gets written to the device:

    Click image for larger version

Name:	code.JPG
Views:	8
Size:	83.5 KB
ID:	113961






    Click image for larger version  Name:	Device.JPG Views:	2 Size:	11.9 KB ID:	113951
    Attached Files
    Last edited by techme; 06-14-2018, 07:15 AM.

    Comment



    • #3
      Techme Thanks for the quick reply. I'll try that today. Thanks again.

      Comment



      • #4
        Techme What did you use to catch the transmission? I would like it in my tool box.....

        Comment



        • #5
          I could not see the code in the post and there was an odd symbol so I edited and replaced teh code screenshot.

          I used a utility called "Packet Sender" it works really well.

          Comment



          • #6
            Thanks so much........

            Comment

            Working...
            X