Announcement

Collapse
No announcement yet.

Cmore and BRX remote connection

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Cmore and BRX remote connection

    I have in the past been using BRX PLC then running a network Ethernet cable to it so I can access remotely, then connecting to the C-more with the EA-2CBL then running a separate Ethernet cable to the cmore so I can access remotely as well. My question is could I use the POM slot on the BRX to connect to the C-more to the BRX, then run the network Ethernet to the BRX Ethernet port only and still access both the cmore and BRX remotely, or am I doing it correctly by using 2 drops?
    Thanks,


  • #2
    Sorry, no. It sounds like you would like the BRX to act as a switch/router. The C-more and the PLC are both end-devices, so you do need 2 Ethernet cables.
    Last edited by franji1; 07-20-2018, 09:08 AM.
    There are 10 kinds of people in this world, those who know binary, and those who do not.

    Comment



    • #3
      Originally posted by franji1 View Post
      Sorry, no. It sounds like you would like the BRX to act as a switch/router. The C-more and the PLC are both end-devices, so you do need 2 Ethernet cables.
      Okay thanks for the response, just wanted to make sure that was the only way.

      Comment

      Working...
      X