Announcement

Collapse
No announcement yet.

P1000 browser connection refused

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts


  • P1000 browser connection refused

    I have my P1000 on a LAN and I can connect to it with the programming software, but when I try to connect using a web browser pointed at the IP address, it says connection refused. What am I doing wrong?


  • #2
    Are you using a proxy server to connect to the internet?
    If so you will have to bypass the proxy server for loacal addresses.
    Or you might not have the Web Server option enabled in the PLC.

    Comment



    • #3
      Thanks for the reply. My admin tells me there is no proxy server, so it must be something else.

      Comment



      • #4
        You need to have the web server function enabled in the PLC hardware config.
        A connection refused error usually means something along the lines of the port being closed or trying to use the wrong port.

        Comment



        • #5
          I'm not seeing web server, I wonder if the P1000 even has that option?

          Comment



          • #6
            I found it! Thanks for your help!
            Last edited by bitmonkey; 10-17-2018, 11:29 AM. Reason: just saying thanks

            Comment

            Working...
            X