Announcement

Collapse
No announcement yet.

How to do ladder MRX and MWX in PLC BRX with several slaves (CLICK)

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • How to do ladder MRX and MWX in PLC BRX with several slaves (CLICK)

    I have three plc click (slave) and a plc BRX (master) but the ladder logic is not working when i connect the slaves together, the instruction MRX and MWX they give me an error ( operation timed out)

  • #2
    Can you access each slave individually?

    Do all slaves have different addresses?

    Wired correctly?

    Lots of possible failures.

    Comment


    • #3
      if I have access to all the slaves and each port is configured correctly
      I'm using RS232, the addresses are the same in each one, and the connection I think is fine

      Comment


      • #4
        Each individual slave works very well for me but the three of them together are not very slow to respond and there is loss of data

        Comment


        • #5
          Originally posted by ecu95 View Post
          if I have access to all the slaves and each port is configured correctly
          I'm using RS232, the addresses are the same in each one, and the connection I think is fine
          RS232 can't be multi-dropped. You have to use RS485.

          Comment


          • #6
            i did not that

            Comment


            • #7
              Originally posted by ecu95 View Post
              the addresses are the same in each one
              They must have different slave/unit addresses. On serial RS-485, everyone is listening, but only 1 can/should respond. The way they know whether the packet is for them is by the Slave/Unit ID. Hence, all Slave IDs must be unique on the network.

              There are 10 kinds of people in this world, those who know binary, and those who do not.

              Comment

              Working...
              X