Announcement

Collapse
No announcement yet.

Click Basic Need ASCII Out

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Click Basic Need ASCII Out

    I have a system with a Click Basic Ethernet PLC and a C-More HMI installed on Com-2. I use the ethernet port with a wireless router for programming.

    Is there a way to use the ethernet port to transmit ASCII out of the PLC when it is running? Data such as flow rates from the flowmeter.

    I would want to connect via a pc using a terminal program. (Initially - ultimately VPN through cellular to a web site.)

    Thanks!

  • #2
    Click Help Topic CL211
    Ethernet Port
    2 Protocol: This Port only supports the MODBUS TCP Protocol.
    Maybe a Serial-Ethernet adapter.
    I have used GridConnect NET232.
    There are other modules, and opinions on each!
    Last edited by kewakl; 11-02-2018, 06:52 AM.

    Comment


    • #3
      Ok so I probably need a standard click if I want eathernet, C-More and data.

      Comment


      • #4
        I have the plc connected to a switch which in turn is onnected to a range extender. This way I can see the plc on wifi.

        Also so connected to the switch is a usr-tcp232-410s; this is a tcp to either rs232 or rs485.
        i have a temp sensor connected on rs485 which I can access from plc using modbus protocol. I can see the temp value on computer and if I had a modbus tcp hmi I could send data from plc to it.
        you can send ASCII either vie modbus ASCII or via rs232 or rs485. The only concern is wether you block a plc port for that or not.

        Comment

        Working...
        X