Announcement

Collapse
No announcement yet.

keyence to productivity plc

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts


  • keyence to productivity plc

    trying to communicate with a keyence iv-hg10 vision sensor and keyence sr-1000 code reader over eithernet to productivity plc. can anyone help?


  • #2
    https://www.youtube.com/watch?v=yzzM_AGAJo8

    Pertinent info from 2:40 to 3:30 mark

    Can't find much on the SR-1000. There is an EDS file for teh SR-750, but I am not registered on Keyence so can't download.

    Comment



    • #3
      I actually have a project where i am going to be using several SR-1000W bar code scanners. there is an EDS you can download from there web sight and with the manual it doesn't look that difficult at all.

      it doesn't look like the tags will import and set up everything as nicely as they set it up for Allen Bradley controllogix platform but it should be entirely workable with out it. i am going to E-mail my contact at Keyence and see if they can make a CSV for the productivity series. I don't think it should be all that hard for them to do

      Comment



      • #4
        I had a bit of spare time. it wasn't hard at all to make a tag import CSV for the productivity series.

        I made sure to set up the IO words and expand to bit level the correct words. Export the tags and then open it up in a spread sheet program. Open up Keyences tag spread sheet and copy the comments to the correct bits and words. (Remember Allen Bradley starts arrays at 0 and the productivity series starts at 1)
        Attached Files

        Comment

        Working...
        X