Announcement

Collapse
No announcement yet.

ControlLogix Lxx using Productivity 3000 I/O

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • ControlLogix Lxx using Productivity 3000 I/O

    What is the best way to have a ControlLogix processor talk to P3000 I/O? The system currently has a main rack w/ a P3-550 CPU. It is talking to several racks via P3-RX I/O adapters. It is also talking to GS2 drives via GS-EDRV100 modules. The Client mandates the ControlLogix processor. Existing I/O is OK to keep using.

    Do the RX scanners talk Modbus TCP? I'm thinking a HMS Anybus adapter would work if that is the case.

    If they don't, do I use the 550 CPU as an Ethernet/IP adapter and map the I/O?

    Thanks,

    Tony


  • #2
    I would use the 550 as ethernetip adapter to the ab.

    Comment

    Working...
    X