Announcement

Collapse
No announcement yet.

What is the maximum cable length I can use on a Direct 05

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • What is the maximum cable length I can use on a Direct 05

    0
    Using rj12 on port 1
    0%
    0
    From computer to PLC
    0%
    0


  • #2
    Port 1 is RS-232 and can be used as a slave only for KSequence, Modbus RTU, or Directnet. Maximum recommended distance per the manual is 15 meters

    "You will need to make sure the network connection is a 3-wire RS–232 type. The recommended cable is AutomationDirect L19772 (Belden 8102) or equivalent. Normally, the RS–232 signals are used for communications between two devices with distances up to a maximum of 15 meters."

    https://cdn.automationdirect.com/sta...er/d0userm.pdf

    Comment



    • #3
      Is there a correct answer to this poll?

      Comment

      Working...
      X