Announcement

Collapse
No announcement yet.

BRX Do-More Ethernet Timeout and Retry Settings for Bad Connections

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • BRX Do-More Ethernet Timeout and Retry Settings for Bad Connections

    I just recently came across a setting that I needed to adjust due to bad/long latency internet connection. I wasn't able to download a program update with the factory settings of TCP timeout 100ms and retry 1, I had to change to 250ms and timeout 3. Is this acceptable to do in a production environment?

  • #2
    As long as it works well, sure. The link info page gives you link stats. I would encourage you to keep an eye on them.

    Comment


    • #3
      Thanks BobO. This has been working well and has since jumped networks several times, now back on a good connection (low delay 10-20ms) and haven't had any issues.

      Comment


      • #4
        Just a follow up on this, everything is still working well, no issues when jumping between networks now, able to see status without a disconnection even on "bad" connections

        Comment

        Working...
        X