Announcement

Collapse
No announcement yet.

P3000 IP Address by program

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • P3000 IP Address by program

    Is there a way, or soon to be a way to configure the External Ethernet IP parameters under program control. Something similar to the IBOX IP Setup in Direct Soft.

    I'm doing a large project that will end up in China that will have 3 PACs communicatiing with each other and other devices. If I can control the IP address from the program. I can utilize the large program space of the PAC to allow only 1 program code for all 3. I would use some jumpers hardwired to a a couple of the inputs to select which IP and which tasks will be active.

    This way, I can give the customer 1 USB Flash Drive for program uploads and he won't have to juggle between them. And especially, when I send upgrades via email, since the file name for all 3 PACs must be the same, he won't accidently load the wrong one.

    I've done this in the past with 06 ad 260's and would like to continue with the PAC
Working...
X