Announcement

Collapse
No announcement yet.

C-more EA9 software v6.41 (Released April 25, 2018)

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • C-more EA9 software v6.41 (Released April 25, 2018)

    Product: C-more software (EA9 panels)
    Version: 6.41
    Release Date: April 25, 2018

    AutomationDirect has released firmware and programming software version 6.41 for the C-more EA9 series touch panels, EA9-PGMSW.

    The software is available at http://support.automationdirect.com/products/cmore.html

    This version includes the following New features, Improvements and Bug Fixes:

    New Features:
    1. Added System Tags for Panel IP Address and Remote IP Address
    2. Added GS4 Drive and PLC Drivers

    Improvements:
    1. Recipe sheet – made menu buttons larger on higher resolution models

    Bug Fixes:
    Software
    1. Cannot open Backup File from previous versions
    2. Background screen can be checked but no screen selected - causes error on screen image export
    3. Project backed up onto USB or SD Card randomly cannot be Restored
    4. Simulator- When simulation is started the virtual storage folders are not created
    5. Random Password keypad position property is not retentive
    6. Object Rotation Base Point not kept when project saved
    7. Email Client Setup Dialog typo - "Enctypted" should be "Encrypted"
    8. Software crashes when opening older project-Windows 7 only
    9. Static Text Object - Parts List - Sample-2 and Sample 3 cause strange behavior when saving project
    Firmware
    1. Bitmap Button pressed behavior not consistent
    2. Clock Source Internal with Productivity Series driver does not write to the PLC
    3. Recipe Not Saving Edits
    4. Current Screen Number not updating when screen is changed by Event Manager

    To download C-more software, please use this link: http://support.automationdirect.com/products/cmore.html
Working...
X