Announcement

Collapse
No announcement yet.

C-more EA9 software v6.42 (Released November 26, 2018)

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • C-more EA9 software v6.42 (Released November 26, 2018)

    Product: C-more software (EA9 panels)
    Version: 6.42
    Release Date: November 26, 2018

    AutomationDirect has released firmware and programming software version 6.42 for the C-more EA9 series touch panels, EA9-PGMSW.

    This version includes the following Bug Fixes:

    Bug Fixes
    Software
    1. Remote Link List getting corrupted and showing the wrong links after adding and deleting links.
    2. Screen Tab - Background Color not accessible is Screen Resolution set to 125%
    3. Object Library Keyboard - Remove CAP and fix character displayed with the Comma Key Button

    Firmware
    1. Popup Screens on Background screen not working after first use
    2. Popup Screen causing simulator and panel to crash
    3. Screen(s) may not properly be updated/displayed after the screen change, if the screen is used on Event Manager as an event trigger.
    4. Simulator crash when packet sent to open Remote Access port 11102
    5. Event Manager Multi Tag Event Logic not working correctly
    6. Recipe Sheet – Read PLC causes an unhandled exception

    To download C-more software, please use this link: http://support.automationdirect.com/products/cmore.html
Working...
X