Announcement

Collapse
No announcement yet.

Label Printing

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Label Printing

    Hey All,

    I really need help. I am trying to print a label using a DL05 or DL06 connected to a serial label printer. Zebra uses EPL or ZPL language depending on which model you are using. HAS ANYONE DONE A PRINTING APPLICATION? if so can you guide me in the right direction or maybe even provide a sample code.

    Mayur Patel
    (630)776-4230

  • #2
    I use the ZPL language, Here is a sample of a string I just sent out my DoMore to a zebra:

    ^XA^PW800 ^LL800^FO190,20^ADN,30^FDAuto Picking Ticket^FS^FO280,80 ^ADN,60,30,^FDBIN 8^FS^FO250,130^ADN,40^BC,70 ^FD 508339^FS ^FO140,280^ADN,20,10^FDSKU LOC Ordered Packed^FS^FO100,310^ADN,30^FD CU103 1233 -2 -2 ^FS^FO100,370^ADN,30^FD CU125 1553 -1 -1 ^FS^FO100,430^ADN,30^FD OML107 1434 -1 -1 ^FS^FO100,490^ADN,30^FD ON108 4135 -1 -1 ^FS^FO0,580^ADN,30^FDTotals: 4 5 5 ^FS ^XZ

    Hopefully this gives you an Idea of the printing layout, but when it comes to the DL06, I have not printed with anything but a CoProcessor from the DL legacy line.
    Sorry I can't be more help, maybe if you could post what you have so far, myself or someone else on here can help you out.
    Circumstances don't determine who we are, they only reveal it.
    Jason Wolthuis

    Comment


    • #3
      Thanks PLCNUT.

      Here is the sample:

      PLC 06

      // Rung 1
      // Address 0
      STRN SP116
      AND C10
      STRND C10
      CNT CT0 K6

      // Rung 2
      // Address 6
      STRE CTA0 K1
      PRINT K0 K0 K2 """test 1"""

      // Rung 3
      // Address 14
      STRE CTA0 K2
      PRINT K0 K0 K2 """test 2"""

      // Rung 4
      // Address 22
      STRE CTA0 K3
      PRINT K0 K0 K2 """test 3"""

      // Rung 5
      // Address 30
      STRE CTA0 K4
      PRINT K0 K0 K2 """test 4"""

      // Rung 6
      // Address 38
      STRE CTA0 K5
      PRINT K0 K0 K2 """test 5$R$L"""

      // Rung 7
      // Address 48
      STRE CTA0 K6
      RST C10

      // Rung 8
      // Address 51
      END

      // Rung 9
      // Address 52
      NOP


      I would replace:
      test1= ""
      test2="N"
      test3="A50,0,0,1,1,N,"HI"
      test4= "P1"

      Am on the right track? i cant get the sp116 bit to be busy so it writes the different ascii out....

      Comment

      Working...
      X