Announcement

Collapse
No announcement yet.

Pneumatic brake control (tension maintainer)

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • #16
    Originally posted by e2dad View Post

    The brx model I am using is BX-DM1E-18ED13. It says Minimum Pulse Width = 0.5 μs - High Speed.

    Since I have two different types of analog signals, would the negative for both be used in terminal "1C" or common in the W (analog) terminal block section of plc?
    High speed discrete input has nothing to do with analog speed, and analog speed has nothing to do with the process speed. What I'm referring to is the latency and response time of the machine components. The PLC is likely fast enough, but I doubt whether the machine can hold +-10lbs even if the PLC speed was infinite.

    Comment

    Working...
    X