Announcement

Collapse
No announcement yet.

Click V2.6 issue

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Click V2.6 issue

    Through serendipity of answering another post, I think I found an issue with the Click software V2.6. THIS is the thread and scroll to response #9. It appears the math instruction will not solve to a float. I know it worked previously in an application coded with V2.1. For convenience, I've attached the program in question.
    Attached Files
    Why worry? If you've done the best you can, worrying won't make it any better

    - Walt Disney

  • #2
    Your project seems to solve for a float just fine here. I'm not using the same model number you're using and I changed the X1 input to one I could easily toggle. If you change your logic to Always_On, does it work then?
    Click image for larger version

Name:	CyclesPerMin.JPG
Views:	108
Size:	156.9 KB
ID:	129377

    Comment


    • #3
      I discovered my issue is the Click model; it has analog I/O, and DF1-DF6 are dedicated to those points. If had chosen DF10 say, I'm certain it would have worked.
      Why worry? If you've done the best you can, worrying won't make it any better

      - Walt Disney

      Comment

      Working...
      X