Announcement

Collapse
No announcement yet.

SOLO Process Temperature Controller

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • SOLO Process Temperature Controller

    I have just finished a post and thought that I would share this with the community.

    Here is an excerpt from the post...

    The recommended screen resolution for the Solo configuration software is 1024 x 768. If you do not have this resolution then there is another program that will allow us to create a shortcut to this program and change our default resolution. After we exit the program, our screen resolution will return to its original state.

    Reso is a free application that works well. It can be downloaded at the following URL link:
    http://www.bcheck.net/apps/reso.htm

    Download the exe file (reso.exe) into the same extracted folder that you have the ADC1105.exe file.

    Read the rest of the post...

    Let me know what you think.
    Thank you,
    Garry
    http://www.accautomation.ca


  • #2
    Thanks for the info.

    I have several of these in use and just programming via the panel interface.

    Comment

    Working...
    X