Announcement

Collapse
No announcement yet.

Thermocouple Range

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Thermocouple Range

    AD Type J and K thermocouples appear not to have ranges below 0C. Most Type J and K by other suppliers do. Comment?

  • #2
    Great question. Our AD Type J and Type K thermocouples are supplied to meet the ASTM E230 Standard Limits of Error which are only defined down to 0C. While our thermocouples can measure below 0C, conformance to the limits of error cannot be guaranteed so the published temperature range is limited at 0C.
    Thanks for the post!
    If you have an urgent issue, please contact AutomationDirect's Technical Support team at 1(800) 633-0405 or (770) 844-4200. Thank you

    Comment

    Working...
    X