Announcement

Collapse
No announcement yet.

Multiple supplies for dc inputs?

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Multiple supplies for dc inputs?

    Hi,

    Looking over the spec sheet for the C0-01DD2-D and it shows 2 separate 24vdc supplies for Y1-Y4 and Y5-Y6. Why can't i use (1) 24v supply for Y1-Y6? I am looking to power 6 small signal reed relays at .012 coil amps per relay? Is it an issue to feed V1 and V2 from the same supply?

    Thanks,
    Adam


  • #2
    That's perfectly fine. They are just allowing you flexibility for when you do need to use 2 separate supplies.

    Comment



    • #3
      Thank you sir!

      Comment



      • #4
        Can I use a C0-01AC supply both the C0-01DD2-D inputs and outputs? I know i have to watch the current rating of the ps.
        The inputs are contact closures from an external relay.
        The outputs feed 24v small signal relays.

        Thanks,
        Adam

        Click image for larger version

Name:	Power Supply.png
Views:	1
Size:	139.0 KB
ID:	104638

        Comment



        • #5
          Yes, as long as you do as you mention - watch the current ratings.

          Comment

          Working...
          X