Announcement

Collapse
No announcement yet.

PID control on Productivity 1000 for Home Brewing

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • #16
    Didn't even think about the average function spanning over the entire time of the brew day. Putting the timer on makes sense. Still a little confused about how the timer works to reset the average temp from your example above. Wouldn't the input of the AVERAGE command have to be reset every 5 seconds? When I read it, it looks like it is just forcing a rewrite of the value for the output over and over every 5 seconds. Maybe I am looking at this too hard. Still trying to understand how all this works.

    This is what I put in my program. Seems to work, but I don't have a good way of testing it over a large temperature span as of yet to see if it averages correctly. I trust you are right, it's just my inexperience that has me a little confused.

    Click image for larger version

Name:	Average Timer Logic.png
Views:	75
Size:	31.2 KB
ID:	110643

    Comment


    • #17
      Little, i looked at the Average function help and got the equation this function is using and I was wrong. This can be used to smooth a reading. I ran some testing and you can use it just as you are. My bad.

      Comment

      Working...
      X