Announcement

Collapse
No announcement yet.

Analog card counting in 4 problem

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Analog card counting in 4 problem

    Hi All.

    Controlling a Vibration Pan controller from a DL06 PLC with an analog card F0-4AD2DA-1 using the 0-20ma Operator Interface is a Cmore EA9-T7CL-R

    The program is written to control the vibrator from 0 -100% however only certain percentage numbers work.

    For example setting the vibrator at 57% is good 58, 59,60 vibrator is off 61% is good (and faster than 57%) 62,63,64 Vibrator is off 65% is good etc etc.

    Any ideas on what I am doing wrong?


  • #2
    You have a data typing issue. IE your Vibrator Entry is in BCD and your PLC program is expecting binary or vice versa.
    If you have an urgent issue, please contact AutomationDirect's Technical Support team.

    AutomationDirect.com Technical Support: 1(800) 633-0405 or (770) 844-4200 Email Tech Support

    Comment

    Working...
    X