Announcement

Collapse
No announcement yet.

M8: uSD Drive Disabled

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • M8: uSD Drive Disabled

    Hi,

    I sent an update to a customer on an SD card.
    He gets the message on the P2-550,

    M8:uSD DRv
    SAVE/LOAD
    DISABLED
    PRESS ESC

    I have this working on the bench no problems.
    Any ideas ?

    Thanks
    Peter


  • #2
    Project that is in the customers plc does not have the "Enable project transfer to/from SD card" checked. This must be done through GUI.

    Click image for larger version

Name:	SD.PNG
Views:	19
Size:	61.5 KB
ID:	120068

    Comment



    • #3
      Looks like I forgot. I opened my installed program and it says it's enabled but i guess it's not.
      Oh well, i'm sending another system i'll send an extra CPU for that one.

      No way to enable from the CPU?

      Thanks for the very fast response techme.

      Peter

      Comment



      • #4
        No this can only be modified with the GUI on a pc and then downloaded to CPU. If you have it enabled and then load a project from the uSD card that it is disabled in it will also cause it to not work until you re enable with the GUI.

        Comment

        Working...
        X