Announcement

Collapse
No announcement yet.

control valves for Click PLC

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • control valves for Click PLC

    Hi,

    I'm working on a process water polishing skid and I need a couple CPVC mixing valves (1" to 2", water, ambient to 150F, 100psi @ 10gpm) I can interface with an analog Click PLC at a reasonable price since there will be more than a couple of these in the final system.

    Modulated would be the most convenient but if floating fail in place, proportional or something else will be significantly less expensive I'm fine with writing some extra code.

    Does anyone have a recommendation for a manufacturer?

    Thanks, Craig


  • #2
    I think Belimo offers PVC valves. I know they have something that would work - not sure how the price will work out.

    Comment



    • #3
      http://www.valworx.com/category/pvc-ball-valves

      or

      bitorq.com


      My application is a very budget conscious one that requires the brass 1" valve. After searching and searching, these two brands are the most bang for my buck. Not sure if it is your solution with PVC valves, but it would be a good starting point.

      Comment

      Working...
      X