Announcement

Collapse
No announcement yet.

PAC doesn't like the program edits, at first.

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • PAC doesn't like the program edits, at first.



    Ethernet download... First attempt usually works, but . . .
    after 1 or 2 or 3 or more tries, the PAC will usually accept the program.
    The LCD indicates CRC error.....

    Sometimes the PAC simply gives up and asks me for a power cycle by the LCD showing the DOS Spin-Of-Death




    System Config:
    11-slot base P3-550 (3*) 16ND3 (8*) 16TD2
    11-slot base P3-RS (7*) 16AD-2
    11-slot base P3-RS (7*) 16AD-2

    EA7-T12C

    (2*) SE-SW5U
    Attached Files

  • #2
    Please contact our Technical Support team so that they can get the project and see if we can duplicate the issue. Provide software version & P3-550 firmware version. In addition, include steps to cause this issue to happen. Does it happen only during download? Any additional details would be appreciated.
    __________________
    If you have an urgent issue, please contact AutomationDirect's Technical Support team.

    AutomationDirect.com Technical Support: 1(800) 633-0405 or (770) 844-4200 Email Tech Support

    Comment


    • #3
      Changed CPU. Have NOT had this error since..
      1 week.

      waiting for techbox to advise.

      Comment

      Working...
      X