Announcement

Collapse
No announcement yet.

Use of non printable ASCII codes in Text messages

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Use of non printable ASCII codes in Text messages

    For activating a RS232 Display I need to Send (by Port2) strings of code including characters like $00 (NUL) or $05 (ENQ). A full code could be something like ($AA) ($20) ($00) ($05).
    Can this be done other then by using embed ASCII codes? The use of an embed location does not work since I have no way of adding such codes in locations (DS or DH).


  • #2
    You can use the Send Dynamic Text option, just build your "string" message first in TXT addresses. Hex characters can be entered directly using "$00" for null. If you have a changing value then you'll need to go through a DH address first then use Copy to TXT with the Binary option.
    Attached Files

    Comment

    Working...
    X