Announcement

Collapse
No announcement yet.

Pointer help file confusion.

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Pointer help file confusion.

    Attempting to use a pointer but there is some confusion in the the help file. In the sentence is that DSC is an acceptable address type, but in the image below shows DS. I note no DSC address type, so should I assume it's just a typo? - OR - some new hidden address type (for a future PID instruction?) Click image for larger version

Name:	Click help confusion.png
Views:	164
Size:	246.2 KB
ID:	124251
    Why worry? If you've done the best you can, worrying won't make it any better

    - Walt Disney

  • #2
    Hmm, new datatype! Naaah. I would assume a typo. If it weren't a typo, where is the useful DS?
    [EDIT] Other CLICK SW version Help files have the same sentence, but without the 'C' appended to the DS register.
    The 'C' is only in V2.40 - as far as I have checked.

    Still, it leaves one to wonder 'what was a Dev doing mucking about in the help file source?' and is there no 'source diff' flag?
    Last edited by kewakl; 07-26-2019, 06:22 AM.

    Comment

    Working...
    X