Announcement

Collapse
No announcement yet.

Click Ethernet/IP Adapter EDS

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Click Ethernet/IP Adapter EDS

    Is it possible to have multiple Click PLCs on the same network running in Ethernet/IP Adapter mode? I am connecting to Click PLC via CoDeSys. It appears that I can't import different EDS files. I would guess that I could manually configure each one. But the use of the different EDS files would be nice. No EDS file format expert, but it looks like exporting the EDS inside of Click always uses the same identifier.

  • #2
    wouldnt they have to have different ip addresses?

    Comment


    • #3
      I'm only used to importing eds files in Logix Studio 5000. In which you specify the ip address after the module insert.

      Comment

      Working...
      X