Hi, I plan on using a Click 0-10V analog output module to control the speed of a DC motor with an IronHorse Gsd1 series Controller. My quick review of the 2.51 program indicates I can set the speed based on an input with a table of values. Can the output (0-10V) be controlled by values directly written into the program? I only need to know if it is possible, I can do the legwork. I assume it would also work the same, if I used the 1-20 ma inputs used on some DC controls? Thanks
Announcement
Collapse
No announcement yet.
0-10 Analog Out
Collapse
X
-
Just be careful if you're plan on using the Click with current/voltage output. Those combo units ONLY provide 0-5V, instead of 0-10V. If you want to use 0-10V, you have to go with an analog voltage only output Click.Why worry? If you've done the best you can, worrying won't make it any better
- Walt Disney
Comment
Comment