Announcement

Collapse
No announcement yet.

Getting started with discrete input

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Getting started with discrete input

    Hi guys,

    I am very new to PLC programming using Click PLC. I rencently purchased a Click PLC C0-12DD2E-2-D.

    I made a very small to program to test a sensor (on X001). As far as i go, the PLC cant seem to read the input.

    I then directly put on X004 the 24VDC and verified it using my multimeter. The voltage is 23.97 VDC.

    I cant see to find what I am doing wrong. Could it be a configuration parameter?
    Can anyone help me finding the problem?

    I will add picture of my "program" and my configuration.
    I updated the firmware and selected the proper PLC.

    Thanks!

    Click image for larger version

Name:	program.PNG
Views:	96
Size:	101.0 KB
ID:	129579

    Click image for larger version

Name:	config.PNG
Views:	57
Size:	126.1 KB
ID:	129580
    Click image for larger version

Name:	hiigh_speed_config.PNG
Views:	57
Size:	83.0 KB
ID:	129581

  • #2
    " then directly put on X004 the 24VDC and verified it using my multimeter. The voltage is 23.97 VDC."

    Do you have C1 connected to 0V?

    Comment


    • #3
      I did not. Should I have 0V on C1?
      thanks

      Comment


      • #4
        Please study carefully study the diagrams in the manual. If you don't understand the diagrams let us know.
        thePLCguy

        Bernie

        Comment


        • #5
          Wire C1 and C2 to your 24V common. Happens all the time

          Comment


          • #6
            Hi,

            It did solve my problem.

            Thanks to all for the quick awnsers.

            Comment

            Working...
            X