Announcement

Collapse
No announcement yet.

Reading data in a file created by FILELOG

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Reading data in a file created by FILELOG

    Good Evening All. I am embarrassed to ask but I've never done this with any DoMore: If I use FileLog to write a datapoint to a file, How can I look into that file to see if things are working?



  • #2
    From Do-more Designer menu: PLC->Browse PLC File Systems...

    From Do-more Designer Dashboard: Left click on the SDCard.

    Comment



    • #3
      Thank you BobO!!!

      Comment



      • #4
        Originally posted by BobO View Post
        From Do-more Designer Dashboard: Left click on the SDCard.
        I've always been annoyed that clicking on the SD card by default puts you in the RAM memory viewer, where you then need to click on the menu to load the SD card...

        Comment



        • #5
          Can the USB B port be used in place of the SD card for Data logging?

          Comment



          • #6
            Originally posted by Rick6785 View Post
            Can the USB B port be used in place of the SD card for Data logging?
            Sorry, no. Wrong side of the USB conversation.

            Comment

            Working...
            X