Announcement

Collapse
No announcement yet.

Do-More bit status

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Do-More bit status

    I have a do-more that is reading registers from a remote PLC into V-memory. Say V1000

    some of these registers are integers and some of them are status bits.

    In directlogic i was able to use direct reference to bits in V-memory. eg i could use B1000.1 as a NO contact. I could also write an output to B1000.2 to turn it on or off.

    The Do-more doesnt seem to allow me to have this access?

    Am i missing something?


  • #2
    V1000:n, where n is 0 to 15. This is a bit cast. There are many forms of casts.

    Search 'casting' in help.

    You can also get help with casting by using the Cast Builder in the Element Browser.

    Comment



    • #3
      Thankyou - i knew it would be simple!

      Comment

      Working...
      X